topics
Renesas Launches World’s Most Highly Integrated Advanced Bluetooth Low Energy SoC
Renesas Launches World’s Most Highly Integrated Advanced Bluetooth Low Energy SoC
New SmartBond DA1470x Family Features Small Form Factor with Integrated Applications and 2D Graphics Processors, Voice Activity Detector and Power Management Enables Small Form Factor for IoT Product Designs
June 21, 2022
Renesas DA1470x Highly Integrated Advanced Bluetooth® Low Energy SoC
TOKYO, Japan ―Renesas Electronics Corporation (TSE: 6723) today announced the SmartBond™ DA1470x Family of Bluetooth® low energy (LE) solutions―the world’s most advanced, integrated System-on-Chip (SoC) family for wireless connectivity.
The DA1470x Family is the only solution in the Bluetooth LE space to integrate a power management unit, a hardware voice activity detector (VAD), a Graphics Processing Unit (GPU) and Bluetooth LE connectivity all into a single chip. This combined functionality provides smart IoT devices with the most advanced sensor and graphical capabilities and seamless, ultra-low-power, always-on audio processing. The new family is ideal for wearables like smartwatches and fitness trackers; glucose monitor readers and other consumer medical and healthcare devices; home appliances with displays; industrial automation and security systems; and Bluetooth consoles such as e-bikes and gaming equipment.
“The DA1470x family expands on our successful strategy of integrating more functions, including greater processing power, expanded memory and improved power modules, along with VAD for always-on wake and command word detection,” said Sean McGrath, Vice President of the Connectivity and Audio Business Division in Renesas’ IoT, Industrial and Infrastructure Business Unit. “This feature-packed SoC product family enables developers to push the boundaries of connected consumer and industrial applications and future-proof their IoT products to fit the needs of multiple applications, while optimizing their bill of materials.”
The high level of integration further results in significant cost savings on the Bill of Materials (BoM), enabling cost-effective system solutions. It also reduces component count on the PCB enabling smaller form factor designs and freeing up space for additional components or larger batteries. With less components on the PCB, the reliability of the system is also improved, delivering a further reduction in the total cost of goods sold (COGS) of the end product.
The SmartBondDA1470x Family is already gaining acceptance in the market. For example, the DA14706 is at the heart of the newly launched Xiaomi Mi band 7 with an eye catching 1.62“, 192×490 AMOLED display, 120 sports modes and a 15-day battery life for typical use.
Please follow the link for full article : https://www.renesas.com/sg/en/about/press-room/renesas-launches-world-s-most-highly-integrated-advanced-bluetooth-low-energy-soc