topics
Renesas Ships 1 Billionth Device From RX Family of 32-bit Microcontrollers
Renesas Ships 1 Billionth Device From RX Family of 32-bit Microcontrollers
Renesas Xtreme (RX) Microcontrollers Are Used in Wide Range of Consumer, Industrial and IoT Applications
January 20, 2022
Renesas Ships 1 Billionth Device From RX MCUs
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced that it has delivered more than one billion microcontrollers from the RX Family of 32-bit MCUs, which incorporate Renesas’ proprietary RX CPU core. Since its launch in 2009, the RX Family has expanded to include general-purpose, motor control, touch sensing, and industrial Ethernet applications, and has been adopted in a wide range of consumer, industrial, and IoT applications. In the home air conditioner compressor market, for example, RX MCUs’ outstanding inverter control has led to adoption by more than 70% of major manufacturers around the world.
“As the world’s leading MCU supplier, we are pleased and proud to work with outstanding customers around the world to achieve this significant milestone,” said Roger Wendelken, Senior Vice President in Renesas’ IoT and Infrastructure Business Unit. “RX MCUs with Renesas’ proprietary cores have established a strong position in applications that require power efficiency and true real-time performance.”
RX MCUs deliver high CPU performance due to their sophisticated architecture for embedded systems. Currently, four series of RX MCUs are available (RX100, RX200, RX600, and the high-end RX700) offering a wide range of performance, on-board memory, and a variety of peripheral functions and packages. Following the introduction of the latest RXv3 core in 2018, Renesas is also working on the development of the next core with the aim of surpassing the performance of the RXv3 core.
Please follow link for full article : https://www.renesas.com/sg/en/about/press-room/renesas-ships-1-billionth-device-rx-family-32-bit-microcontrollers