topics
Renesas Unlocks Personalized Air Quality Experiences With Ultra-Low Power ZMOD4510 Outdoor Air Quality Sensor Platform
Renesas Unlocks Personalized Air Quality Experiences With Ultra-Low Power ZMOD4510 Outdoor Air Quality Sensor Platform
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its popular ZMOD4510 Outdoor Air Quality (OAQ) gas sensor platform with an IP67-qualifed waterproof package and a new AI-based algorithm that enables ultra-low power selective ozone measurements. The enhanced ZMOD4510 is the industry’s first fully calibrated, miniature digital OAQ sensor solution with selective ozone measurement capabilities, offering visibility into the air quality in users’ immediate environments for a personalized experience.
Ozone gas is a significant cause of poor outdoor air quality that poses health risks. Based on Renesas’ new ultra-low power firmware, the enhanced ZMOD4510 can detect specific ozone levels – without reporting on other pollutants – while maintaining power consumption under 200 uW. This selective measurement capability allows devices such as smart watches, phones, and smoke detectors to monitor for harmful ozone gasses typically found outdoors but which can drift indoors through open windows and doors. Optimizing the ZMOD4510 for very low power is key to enabling the longer life cycles required for these types of battery-powered devices.
“Measuring outdoor air quality really is about location, location, location, as levels can vary dramatically from street to street and even on opposite sides of the same street,” said Uwe Guenther, Senior Director, Sensing Solutions, IoT and Infrastructure Business Unit at Renesas. “The enhanced ZMOD4510 gives manufacturers the selective high-precision sensing, ultra-small size, and long battery life they need for battery-powered devices like smart watches and phones that offer customers a convenient and customized view of their immediate air quality environment.”
For full article, please follow the link : https://www.renesas.com/sg/en/about/press-room/renesas-unlocks-personalized-air-quality-experiences-ultra-low-power-zmod4510-outdoor-air-quality