topics
Renesas Launches RX23W Module with Bluetooth for System Control and Wireless Communication on IoT Devices
Renesas Launches RX23W Module with Bluetooth for System Control and Wireless Communication on IoT Devices
New Radio Law-Certified Bluetooth Module Combines RX23W MCU, Antenna, and Peripheral Circuits in an Industry-leading Small Package
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the RX23W Module with full Bluetooth® 5.0 Low Energy support for system control and wireless communication on IoT endpoint devices. Featuring the RX23W 32-bit RX MCU supporting fully integrated Bluetooth Low Energy communication, the new RX23W module is equipped with an antenna, oscillator and custom-matched circuit. The new module is certified under Radio Law for multiple countries, including Japan and the United States (Note), and is Bluetooth SIG certified. This eliminates the need for additional RF design work, tuning, or specialized RF knowledge, allowing customers to use the module as it is, shortening new product development time. The very small 6.1 mm x 9.5 mm, 83-pin LGA package makes it possible to design more compact devices with fewer external components, reducing the bill of materials (BOM) cost. This improves the development efficiency of IoT endpoint devices such as home appliance, healthcare and sports and fitness equipment.
The RX23W MCU incorporated in the new module supports full Bluetooth 5.0 Low Energy communication support including long-range and 2 Mbps data throughput. It delivers excellent communication characteristics, with reception sensitivity level of −105 dBm at 125 kbps. Built around Renesas’ RXv2 CPU core, the RX23W MCU provides outstanding computing performance, operating at a maximum clock frequency of 54 MHz together with outstanding power efficiency, making it ideally suited for system control. The RX23W also incorporates Renesas’ exclusive security function, the Trusted Secure IP (TSIP), that provides robust protection against threats to IoT devices such as eavesdropping, tampering, and viruses. In addition, the RX23W MCU has a rich set of peripheral functions that is indispensable to IoT devices, including touch key, USB, and CAN functions.
“As development cycles for IoT devices become shorter, the development burden increases,” said Sakae Ito, Vice President of IoT Platform Business Division at Renesas. “I am delighted that, as we approach the ten-year mark, a wide range of customers have adopted our RX MCUs. We are pleased we can now announce the release of our first Bluetooth communication module based on the Renesas RX MCU, thereby helping to make the development process more efficient.”
Development Environment
The new RX23W module utilizes the same software development environment used for RX MCUs, which means developers can work on both system and communication control at the same time. Smart Configurator enables developers to employ a GUI to generate driver code for peripheral functions and Bluetooth, as well as configuring pin settings. QE for BLE enables developers to generate programs for custom Bluetooth profiles. The Bluetooth Test Tool Suite provides a GUI that allows developers to perform initial wireless characteristics evaluations and Bluetooth functionality verification. These tools are well suited to the various phases of development, providing support for developers from the initial stages through applied product development, and substantially boosting efficiency.
The RX23W Module can be combined with Renesas’ complementary analog and power offerings to create comprehensive solutions for a variety of applications. These “Winning Combinations” showcase the unique capabilities of the RX23W Module and the breadth and depth of Renesas’ product line up. Applications includes a reference design for a Medical Patch that can monitor body temperature, oxygen saturation (SpO2) and heart rate over a Bluetooth connection using RX23W, and a 48V Mobility Solution that can save the mobility battery status and route history by smartphone connection through RX23W.
Pricing and Availability
The RX23W Module is available at the reference price of US$6.60 per 10,000-unit quantities, and mass production and shipping have already begun. A target board for evaluation is also available at a reference price of US$50 per unit, and it is available starting today. For more information on the Renesas RX23W Module, visit: www.renesas.com/rx23w-module
Note: The RX23W Module is certified under the applicable laws of the United States, Canada, the EU, and Japan.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks) Bluetooth is a registered trademark of Bluetooth SIG, Inc. All registered trademarks or trademarks are the property of their respective owners.
____________________________________________________________________________________________________________________________________________________________________________
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.