topics


Renesas Introduces Complete Power and Functional Safety Solution for R-Car V3H ADAS Camera Systems

Renesas Introduces Complete Power and Functional Safety Solution for R-Car V3H ADAS Camera Systems

New Synchronous Buck Pre-Regulator and Safe Seven-Channel PMIC Combine to Reduce Power Loss, System Cost and Design Time

Complete Power and Functional Safety Solution for Renesas R-Car V3H SoC

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced a new power and functional safety solution for systems based on the R-Car V3H system-on-chip (SoC) for advanced driver assistance systems (ADAS) automotive front cameras and driver monitor cameras.

The new solution includes the RAA271050, a 42V synchronous buck ‘pre-regulator’ that accepts the vehicle’s 12V supply and steps it down to an intermediate supply voltage of 3.3V or 5.0V. The RAA271000, a seven-channel PMIC (power management IC), then takes the RAA271050’s output and steps it down further to the various supply voltages needed by R-Car V3H and its peripherals such as LPDDR4 memory. Both devices were developed per the ISO-26262 standard, and can support system safety requirements up to ASIL D. The solution satisfies all the power and functional safety requirements for the R-Car V3H. It provides supply voltages with the current capability to meet all power specifications, including sequence, voltage accuracy, and load step response. For safety, it provides all the necessary power and digital monitoring functions.

Renesas’ new solution provides best-in-class efficiency, with power loss reductions of up to 33 percent compared to competitive PMICs under comparable operating conditions. Lower power loss enables operation at higher temperatures, reducing cooling costs and delivering better reliability. Additionally, the RAA271050 and RAA271000 were designed to match R-Car requirements with no unnecessary overhead, reducing component cost and PCB area. Renesas is providing a reference hardware solution that includes the new components, speeding design time and reducing testing requirements for customers.

“This new power and functional safety solution showcases our power design expertise to offer R-Car V3H customers significant cost savings,” said Niall Lyne, Vice President of Renesas’ Automotive Analog Power and Video Business Division. “And we’re delivering a complete, tested design that enables designers to implement the latest in ADAS camera applications quickly and efficiently.”

Key Features of the R-Car V3H Power Solution
# Programmable Output Voltage, Sequencing, I/O Configuration and Safety Configuration providing flexibility to support R-CAR V3H and an expansive range of SoCs
# Integrated 12-bit SAR ADC with up to 16 external inputs monitors internal and external signals, eliminating the need for an added system ADC
# Dynamic Voltage Frequency Scaling (DVFS) adjusts output voltage to minimize power consumption
# Optional Spread Spectrum Clocking mitigates EMI
# Built-in Support for R-Car V3H SoC Activation streamlines SoC self-test procedures

Complete ADAS Camera Solution
The RAA271050 and RAA271000 are included in a complete ADAS front camera solution featuring the EagleCam camera module from LUPA-Electronics GmbH and Renesas’ R-Car V3H and R-Car V3M system-on-chip (SoC) devices. This “Winning Combination” is an open, turnkey solution that delivers flexible, high-performance perception while shortening time to market and reducing the bill of materials (BOM) cost. More information on this design is available at https://www.renesas.com/EagleCAM.

Availability
The RAA271050 is offered in a 22-lead, 4x4mm QFN package. The RAA271000 is packaged in a 60-ball FCBGA with 0.8mm pitch. Both devices are sampling today and are expected to be fully available in July of this year. Users can visit www.renesas.com/RAA271050 and www.renesas.com/RAA271000 for more information on the new parts.

About R-Car V3H
The highly integrated R-Car V3H SoC supports up to ASIL C metrics safety goals on the real-time domain, reducing the need for an external safety microcontroller (MCU) to manage sensor fusion and final decision actions. The R-Car V3H features a suite of proven IPs that support the perception stack, sensor fusion with radar and/or Lidar, and ISP with up to eight MP cameras support, allowing OEMs and Tier 1s to achieve quicker time to market with lower bill of materials costs. Renesas recently announced significantly improved deep learning performance for smart camera applications, including driver and occupant monitoring systems (DMS / OMS), automotive front cameras, surround view, and auto parking for high-volume vehicles up to Level 2+. More information is available at https://www.renesas.com/us/en/products/automotive-products/automotive-system-chips-socs/r-car-v3h-system-chip-soc-designed-intelligent-camera-deep-learning-capabilities.

About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). Arm, Arm Cortex, and Arm TrustZone are trademarks or registered trademarks of Arm Limited in the EU and other countries. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.

____________________________________________________________________________________________________________________________________________________________________________
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

For further info, please access the link via: