topics
Renesas Extends IoT Security Leadership With PSA Certified Level 2 and SESIP Certification for RA Family Devices
Renesas Extends IoT Security Leadership With PSA Certified Level 2 and SESIP Certification for RA Family Devices
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced both PSA Certified Level 2 and Security Evaluation Standard for IoT Platforms (SESIP) certifications for its RA Family of 32-bit Arm® Cortex®-M microcontrollers (MCUs).
Renesas’ RA6M4 MCU Group devices with the Flexible Software Package (FSP) have been PSA Level 2 certified, expanding on the PSA Certified Level 1 achieved by RA4 and RA6 Series MCUs. Renesas’ RA6M3, RA6M4, and RA4M2 MCU groups have achieved SESIP1 certification with Physical and Logical Attacker certifications.
In addition to these widely recognized industry certifications, Renesas RA MCUs offer customers the ultimate IoT security by combining Secure Crypto Engine IP with NIST CAVP certifications on top of Arm TrustZone® for Armv8-M. RA Family devices incorporate hardware-based security features from simple AES acceleration to fully-integrated crypto subsystems isolated within the MCU. The Secure Crypto Engine provides symmetric and asymmetric encryption and decryption, hash functions, true random number generation (TRNG), and advanced key handling, including key generation and MCU-unique key wrapping. An access management circuit shuts down the crypto engine if the correct access protocol is not followed, and dedicated RAM ensures that plaintext keys are never exposed to any CPU or peripheral bus.
“Renesas understands that security is essential for IoT designers, so we have engineered the RA Family from the ground up with security in mind,” said Roger Wendelken, Senior Vice President in Renesas’ IoT and Infrastructure Business Unit. “These industry certifications augment what is already the most secure device family in the industry for IoT applications.”
“We are glad to work with Renesas on the SESIP and PSA Certified certifications. Renesas RA Family certifications are prime examples of the relevance of security standards for the industry,“ said Carlos Serratos, Senior Director of Strategy, Policy and Advocacy at Brightsight. “From an OEM perspective, there is an increasing awareness of the value of certified devices as a tool for managing risk, and for aligning with multiple device certifications. While this is particularly relevant for devices used in critical infrastructures, it is steadily becoming the norm for the rest of the IoT domain.”
PSA Certified offers a framework for securing connected devices, from analysis through to security assessment and certification. The framework provides standardized resources addressing the growing fragmentation of IoT requirements, ensuring security is no longer a barrier to product development. PSA Certified through a third- party laboratory evaluation of a PSA Root of Trust (PSA-RoT), PSA Certified Level 2 provides evidence of protection against scalable software attacks. Evaluation Labs use vulnerability analysis and penetration testing of the PSA-RoT to establish if the nine security requirements of the PSA-RoT Protection Profile have been met.
SESIP is an optimized version of Common Criteria methodology (ISO 15408-3) for the evaluation of IoT components and connected platforms. SESIP defines a catalogue of Security Functional Requirements (SFRs), which the product developer can use to build their secure device, scaling appropriately for their specific threat model and use case. SESIP also incorporates and refines Common Criteria Security Assurance Requirements (SARs), including the requirement ALC_FLR.2 Flaw Reporting Procedures, which Renesas addresses with its Renesas PSIRT (Renesas Product Security Incident Response Team) process and public web interface. Specifically designed for SFR reuse and mapping to other certifications, the SESIP methodology enables product developers to pursue appropriate certification of their device to other industry-standard certifications such as IEC 62443.
About Brightsight
Brightsight is the number one independent security lab in the world. With over 35 years of experience evaluating IT products, Brightsight is the preferred business and advisory partner for certification and security evaluations of Smartcards, ICs, HSMs, System on Chip, Payment terminals, Smartmeters, Mobile Payment, IoT, Automotive and Biometric solutions. With offices in the Netherlands, Spain, China and France, Brightsight helps customers in getting their products ready and in compliance with the latest security regulations and requirements. Learn more at Brightsight.com.
About Renesas’ RA MCU Family
The RA Family ecosystem accelerates the development of IoT applications with core technologies such as security, safety, connectivity and HMI. Designing with RA MCUs makes it easy for engineers to develop Internet of Things (IoT) endpoint and edge devices for industrial and building automation, metering, healthcare, and home appliance applications. The RA Family includes the RA2 Series (up to 60 MHz), RA4 Series (up to 100 MHz), RA6 Series (up to 200 MHz), and the single/dual-core RA8 Series, to be released later. More information about the RA MCU Family is available at www.renesas.com/RA.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks) Arm, Arm Cortex, and Arm TrustZone are trademarks or registered trademarks of Arm Limited in the EU and other countries. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
For further info, please access the link via: