topics


Renesas Expands RF Portfolio to Cover Complete Signal Chain for Macro Base Stations

Renesas Expands RF Portfolio to Cover Complete Signal Chain for Macro Base Stations

Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today strengthened its industry-leading RF portfolio for traditional macro base transceiver stations (BTS) with four new high-reliability, high-performance devices, offering customers access to a complete RF signal chain solution. This expansion includes the industry’s first quad-channel F4482/1 TX variable gain amplifiers (VGA) and the F011x family of dual-channel first-stage low noise amplifiers (LNA). The new device set also includes the F1471 RF driver amplifier – the first high-power pre-driver with P1dB of over 1/2W – and the F2934 RF switch with higher isolation in a smaller package for digital predistortion (DPD) feedback path.

The expanded RF lineup delivers the high performance, high reliability, flexibility, and smaller form factor demanded by 5G Macro BTS systems. These new RF devices perform well across a wide range of environmental conditions and frequency bandwidths, and integrate Renesas’ Smart Silicon™ innovations, which enable smaller footprints for a given function – a key advantage for the large number of antenna paths required for each system.

“As the 5G transition picks up speed, we have upgraded our Macro BTS portfolio of receive and transmit chain components with higher performance and higher integration,” said Naveen Yanduru, Vice President of RF Communications, Industrial and Communications Business Division at Renesas. “We continue to bring new circuit design advancements to the market and are excited to introduce these new devices to address the complete RF signal chain and enable customers to be 5G ready as they bring their next-generation Macro BTS systems to market.”

Macro BTS customers can combine these new devices with the recently released F1490 high-gain RF amplifier and highly integrated F0443 RX VGA for complete RF signal chain solutions.

For further info, please access the link via: https://www.renesas.com/sg/en/about/press-room/renesas-expands-rf-portfolio-cover-complete-signal-chain-macro-base-stations