topics


Renesas Accelerates ADAS and Automated Driving Development with Best-in-Class R-Car V3U ASIL D System on Chip

Renesas Accelerates ADAS and Automated Driving Development with Best-in-Class R-Car V3U ASIL D System on Chip

Today, Renesas Electronics Corporation, a premier supplier of advanced semiconductor solutions, unveiled the R-Car V3U – a best-in-class ASIL D system on chip (SoC) for advanced driver assistance systems (ADAS) and automated driving (AD) systems. Delivering a groundbreaking 60 TOPS with low power consumption for deep learning processing and up to 96,000 DMIPS, the R-Car V3U is built for the performance, safety, and scalability (up and down) demands of ADAS and AD architectures driving next-generation autonomous vehicles.

The new R-Car V3U is the first SoC using the R-Car Gen 4 architecture within the open and flexible Renesas autonomy platform for ADAS and AD. With the launch of R-Car V3U, the platform is now ready to offer complete scalability from entry-level NCAP applications up to highly automated driving systems.

“We are excited to introduce the newest generation of our popular R-Car SoCs for the next generation of ADAS and AD vehicles,” said Naoki Yoshida, Vice President, Automotive Digital Products Marketing Division at Renesas. “The R-Car V3U leverages assets developed on previous-generation devices, such as ADAS and Level 2 perception stack with the R-Car V3M and R-Car V3H, along with the Renesas autonomy platform, to offer a smooth migration path to single-chip Level 3 automated driving with short development turnaround and safe production launch.”

For further info, please access the link via: https://www.renesas.com/sg/en/about/press-room/renesas-accelerates-adas-and-automated-driving-development-best-class-r-car-v3u-asil-d-system-chip