topics
Renesas Expands ZMOD4410 Indoor Air Quality Family With Industry’s First IP67 Waterproof Sensor for High-Humidity Environments
Renesas Expands ZMOD4410 Indoor Air Quality Family With Industry’s First IP67 Waterproof Sensor for High-Humidity Environments
Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its popular ZMOD4410 Indoor Air Quality (IAQ) sensor platform with the industry’s first software-configurable IP67-qualified waterproof option for IAQ applications operating in wet or dirty environments such as kitchens, bathrooms, and hospital rooms, where they are frequently exposed to water, oils, and dust.
The firmware-configurable waterproof ZMOD4410 sensor features a unique hermetically sealed package that protects the sensor from water and dust with a hydrophobic and oleophobic material that is permeable to humidity and volatile organic compounds (VOCs) at the same time. By combining IP67-rated packaging with the industry-leading accuracy and reliability that the ZMOD4410 platform is known for, Renesas enables new, low-power IAQ applications that operate in splash zones, while maintaining the high precision and flexibility customers need to customize their systems and eliminating the need for expensive waterproofing systems.
For further info, please access the link via: https://www.renesas.com/sg/en/about/press-room/renesas-expands-zmod4410-indoor-air-quality-family-industry-s-first-ip67-waterproof-sensor-high