topics
Renesas’ Intersil Brand 14-Bit, 1-MSPS ADC Delivers Best-in-Class Radiation-Hardened Performance for Satellites, Manned Spacecraft, and Lunar Space Missions
Renesas’ Intersil Brand 14-Bit, 1-MSPS ADC Delivers Best-in-Class Radiation-Hardened Performance for Satellites, Manned Spacecraft, and Lunar Space Missions
Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the industry’s highest performance single-chip 14-Bit, 1-MSPS successive-approximation-register (SAR) analog-to-digital converter (ADC) for radiation-hardened (rad-hard) space applications. Renesas’ Intersil brand ISL73141SEH delivers best in class dynamic and static performance, including signal-to-noise ratio (SNR), effective number of bits (ENOB), integral non-linearity (INL) and differential non-linearity (DNL). The ADC fully resets after every sample, clearing any errors that result from a single event upset (SEU) due to heavy ion radiation during spaceflight.
The ISL73141SEH is one of the key signal-path building blocks in long duration geosynchronous / geostationary Earth orbit (GEO) communication satellites and manned spacecraft, including lunar space missions. By delivering the industry’s best dynamic and static performance, the new 14-bit ADC accurately captures real-world analog transmissions and converts them for processing in the digital domain. The ISL73141SEH ADC is one of seven ICs, including rad-hard temperature sensor, multiplexer, quad op amp, ADC driver, LDO and voltage reference to form a complete sensor interface signal chain solution that accelerates telemetry, tracking, and control (TT&C) and flight computer system development.
“The ISL73141SEH offers satellite and spacecraft manufacturers the ultimate in ADC performance combined with a best-in-class sensor interface signal chain,” said Philip Chesley, Vice President, Industrial and Communications Business Division at Renesas. “Our space-grade 14-bit ADC delivers significantly better data converter performance than any other competing solution, and it is backed by six decades of leadership in radiation performance testing and characterization that gives spaceflight customers the mission assurance they demand.”
The space-grade ISL73141SEH is fully characterized for enhanced low dose rate-sensitivity (ELDRS) radiation performance up to 75krad(Si) for total ionizing dose (TID) and linear energy transfer (LET) up to 86MeV*cm2/mg for single event effects (SEE). The SEE testing also shows no single event latch-up (SEL) or single event burnout (SEB). In addition, single event transients (SETs) have also been mitigated by testing at an LET range up to 86MeV*cm2/mg.
For further info, please access the link via: https://www.renesas.com/sg/en/about/press-room/renesas-intersil-brand-14-bit-1-msps-adc-delivers-best-class-radiation-hardened-performance