topics


Renesas I3C Bus Extension and SPD Hub Devices Qualified for ASPEED AST2600 Baseboard Management Controller

Renesas I3C Bus Extension and SPD Hub Devices Qualified for ASPEED AST2600 Baseboard Management Controller

Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced that ASPEED Technology has qualified the Renesas I3C IMX3102 2:1 bus multiplexer, IMX3112 1:2 bus expander, and DDR5 SPD Hub SPD5118 for its cutting-edge AST2600 Baseboard Management Controller (BMC) designed for use in data centers and embedded platforms and applications. Renesas is the first I3C partner selected for ASPEED’s AST2600 BMC Approved Vendor List (AVL), enabling an easy migration path for customers shifting their DDR5 platforms and boards from I2C or other legacy expansion specifications to the new high-speed I3C specification.

The Renesas I3C re-driver and expander products include many features that enable customers to develop their applications more efficiently and cost effectively compared with existing solutions. These include in-band switching control via I2C/I3C commands to switch over, level-shifting capability with master devices working in 3.3V while peripherals work in 1.0V, and reduced bill of materials costs by eliminating additional circuitry, such as pull-up resistors. Combined with the ASPEED AST2600 BMC, Renesas I3C devices provide optimized, high-speed, and system cost-centric combination solutions to meet customers’ application needs.

For further info, please access the link: https://www.renesas.com/sg/en/about/press-center/news/2020/news20200929.html