topics
Renesas Introduces DDR5 Data Buffer for High-Performance Server and Cloud Service Applications
Renesas Introduces DDR5 Data Buffer for High-Performance Server and Cloud Service Applications
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions and the industry leader in memory interface products, today announced a new high-speed, low-power DDR5 data buffer for data center, server, and high-performance workstation applications.
Advancements over the past few years in real-time analytics, machine learning, HPC, AI, and other memory and bandwidth-hungry applications have fueled explosive growth in server memory bandwidth requirements. The new JEDEC-compliant DDR5 data buffer 5DB0148 from Renesas enables significantly higher speeds and lower latency for load-reduced dual inline memory modules (LRDIMMs) that have become the cornerstone memory technology for this new class of applications. The first generation of DDR5 LRDIMMs based on Renesas components enable a bandwidth increase of more than 35 percent over DDR4 LRDIMMs operating at 3200 MT/s.
The Renesas DDR5 Data Buffer maximizes channel eye opening for systems that are heavily loaded through a combination of capacitive load reduction, data alignment, and signal recovery techniques. This allows server motherboards with a large number of memory channels and slots and complex routing topologies to run at maximum speed, even when fully populated with high-density memory. Additionally, improvements in the DDR5 modules definition allow for lower power supply voltages (1.1V vs 1.2V in DDR4), on-DIMM voltage regulation, and implementation of advanced control plane architectures with the use of the SPD Hub and modern control bus communications such as I3C
For further info , please access the link via: https://www.renesas.com/sg/en/about/press-center/news/2020/news20200909.html