topics


Renesas Electronics Launches RX72M Group of Microcontrollers with EtherCAT® Support for Industrial Applications

Renesas Electronics Launches RX72M Group of Microcontrollers with EtherCAT® Support for Industrial Applications

TOKYO, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced the RX72M Group of RX microcontrollers (MCUs) featuring an EtherCAT® slave controller for industrial Ethernet communication. The new flagship product group for the Renesas RX family offers a high-performance, single-chip MCU solution with large memory capacities for industrial equipment requiring control and communication functions such as compact industrial robots, programmable logic controllers, remote I/O, and industrial gateways.

The use of EtherCAT in industrial Ethernet is growing fast, and is currently used on dedicated MCUs, ICs, and high-end system-on-chip (SoC) devices specialized for EtherCAT communication. The new RX72M Group achieves the superior performance of a 1396 CoreMark® score (Note 1) at 240MHz as measured by EEMBC® Benchmarks, and it is capable of both application processing and EtherCAT communication. Combining a motor-control MCU with on-chip EtherCAT slave functions allows industrial application developers reduce their bill of materials (BOM) and support the miniaturization levels required for industrial equipment design.

For full article, please access link : https://www.renesas.com/sg/en/about/press-center/news/2019/news20190606.html