topics


Renesas Electronics Unveils Easy, Cost-Effective Liquid and Solid Material Detection Solution for Industrial, OA, and Home Appliances

Renesas Electronics Unveils Easy, Cost-Effective Liquid and Solid Material Detection Solution for Industrial, OA, and Home Appliances

TOKYO, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced its Material Detection Solution, which can detect materials or liquids easily and cost effectively without sensors by connecting electrodes using Renesas’ RX130 capacitive touch-key microcontrollers (MCUs). Replacing the sensors with this electrode approach contributes to lower bill of materials (BOM) costs while enabling detection at multiple points using a single chip. This allows industrial equipment, OA equipment, and home appliance manufacturers to explore detection systems for cost-constrained applications.

Renesas’ touch-key MCUs feature a capacitive touch sensor unit specialized for capacitance measurement with extremely high sensitivity and high noise resistance. This enables the Material Detection Solution to easily detect the presence or absence of a powder such as vacuum cleaner dust, a liquid such as refrigerator and coffee maker, or material such as paper by measuring the capacitance between electrodes to the MCU. The increase or decrease of the powder, liquid, or material will change the capacitance value between the electrodes.

“Sensor systems are an indispensable element in our customers’ application development efforts, and we are excited to add capacitive touch solutions with different capabilities that enable new use cases,” said Shigeki Kato, Vice President of Renesas’ Enterprise Infrastructure Business Division, Industrial Solution Business Unit. “With our new capacitive touch-based detection systems, customers can expand their sensing function range while taking advantage of reduced BOM cost and improved detection accuracy.”

As sensor-based technology proliferates in industrial equipment, OA equipment, and home appliances, the demand for different types of sensor solutions is rapidly increasing to address diverse sensing needs. Applications require fine-grained sensing for predictive maintenance capabilities. For instance, printers are required to detect the remaining amounts of consumable materials and inform users in advance when replacements are required. Vacuum cleaners also need to manage the accumulation of dust retained by vacuum cleaner filters in order to perform efficient cleaning. This provides improved device functionality and increased user convenience.

Although these applications can be implemented by using various types of sensors, such as pressure sensors for detecting physical objects, photosensors, IR sensors, and CMOS sensors, the use of multiple sensors creates additional cost and heavy development burdens.

For full article, please follow the link : https://www.renesas.com/sg/en/about/press-center/news/2019/news20190423.html