topics
Renesas Electronics Simplifies Development of USB PD and USB-C™ Battery Charging Applications with New Reference Designs
Renesas Electronics Simplifies Development of USB PD and USB-C™ Battery Charging Applications with New Reference Designs
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced two new reference designs that simplify and speed the development of USB Power Delivery (PD3.0) and USB-C™ battery charging applications such as USB-C computing hubs, power banks, car chargers, SSD enclosures, point of sale (POS) printers, and desktop displays. The RTK-251-1PowerBank3 and RTK-251-BuckBoostConverter2 are USB-IF PD3.0 certified design kits, and represent the first in a new series of reference designs for applications implementing the USB Type-C™ power and data connection standard.
The RTK-251-1PowerBank3 board is a 3-cell (series connected) Li-ion battery power bank reference design that employs the R9A02G011 USB PD3.0 controller and ISL95538B buck-boost Narrow Voltage Direct Charging (NVDC) battery charger. Ideal for USB-C multi-battery-cell power banks, the reference design board includes one USB Type-C port that supports the Dual Role Power (DRP) feature, delivering power in both directions via power source and power sink modes. When the power bank is in sink mode, it requests 5V, 9V, 15V, or 20V from a USB PD3.0 provider such as an AC adapter. When the power bank is in source mode, the Li-ion battery supplies 5V up to 20V requested from a PC, tablet, or smartphone. In addition, the RTK-251-1PowerBank3 changes its DRP role based on the remaining battery capacity displayed on the board’s LEDs.
The RTK-251-BuckBoostConverter2 is a DC/DC module that employs the R9A02G011 USB PD3.0 controller and the ISL95338 bidirectional buck-boost voltage regulator. The RTK-251-BuckBoostConverter2 reference design board is ideal for USB-C hubs as part of the USB-PD AC adapter connection. It accepts 19V with 4.73A DC input power and produces USB-PD3.0-compatible VBUS output power. The reference design board supports Programmable Power Supply (PPS) and has two USB Type-C receptacles for VBUS power output.
“The RTK-251-1PowerBank3 and RTK-251-BuckBoostConverter2 reference designs significantly speed up customers’ development schedules by providing tested and complete solutions ready to drop into any design,” said Andrew Cowell, Vice President, Battery & Optical Systems Division, Renesas Electronics Corporation. “Renesas’ industry-leading USB-PD and USB-C products enable smaller form factors, faster charging, and higher efficiency for remarkably longer battery life.”
For full article, please follow the link : https://www.renesas.com/sg/en/about/press-center/news/2019/news20190403.html