topics
Renesas Electronics to Release RZ/G Linux Platform Solution Supporting IEC 62443 International Standard for Protection of Industrial Control Systems Against Cyberattacks by EO2019
Renesas Electronics to Release RZ/G Linux Platform Solution Supporting IEC 62443 International Standard for Protection of Industrial Control Systems Against Cyberattacks by EO2019
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced plans to release a security solution based on the Renesas RZ/G Linux Platform that will reduce the amount of time required for users to obtain certification under IEC 62443-4-2, a new international standard for security technologies used to protect industrial control systems from cyberattacks.
In today’s connected world, robust security measures are essential. Cyberattacks on industrial control systems for infrastructure facilities such as manufacturing plants and power stations pose the risk of serious disruption to people’s lives and to the economy. For this reason, the IEC established the IEC 62443 international security standard covering all layers (operators, system integrators, and equipment suppliers) engaged in the manufacturing of industrial control systems and all players (enterprises and organizations involved in industry and public infrastructure). Within this standard, endpoint devices such as sensors and programmable logic controllers (PLCs) must be certified under IEC 62443-4. The certification process imposes a significant burden on developers. It requires them to interpret the difficult standard, to prepare the software and documentation required for certification, and to execute a procedure that requires specialized expertise.
To help developers overcome these certification challenges, Renesas is developing an industrial security solution that supports IEC 62443-4. Together with deliverables through the activities in Civil Infrastructure Platform (CIP™) Project, the Renesas RZ/G Linux Platform security solution will enable users to reduce the time required for obtaining IEC 62443-4-2 certification by as much as six months.
For full articles, please access link via : https://www.renesas.com/sg/en/about/press-center/news/2019/news20190326.html