topics


Renesas Electronics Simplifies Home Appliance Maintenance with Failure Detection e-AI Solution for Motor-Equipped Home Appliances

Renesas Electronics Simplifies Home Appliance Maintenance with Failure Detection e-AI Solution for Motor-Equipped Home Appliances

TOKYO, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the launch of its Failure Detection e-AI Solution for motor-equipped home appliances, featuring the Renesas RX66T 32-bit microcontroller (MCU). This solution with embedded AI (e-AI) enables failure detection of home appliances — such as refrigerators, air conditioners, and washing machines — due to motor abnormality. Property data showing the motor’s current or rotation rate status can be used directly for abnormality detection, making it possible to implement both motor control and e-AI–based abnormality detection with a single MCU. Using the RX66T eliminates the need for additional sensors, thereby reducing a customer’s bill of materials (BOM) cost.

For full article, please access link via : https://www.renesas.com/sg/en/about/press-center/news/2019/news20190121.html