topics
Renesas Electronics’ 32-bit RX65N Microcontrollers with Advanced Security and Graphics Achieves Amazon FreeRTOS Qualification
Renesas Electronics’ 32-bit RX65N Microcontrollers with Advanced Security and Graphics Achieves Amazon FreeRTOS Qualification
08 Jan 2019
TOKYO, Japan – Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the qualification of their RX65N Group of microcontrollers (MCU) with Amazon FreeRTOS, running on Amazon Web Services (AWS). The Renesas RX65N MCU lineup with Amazon FreeRTOS makes it easy for embedded designers to create a more secure end-to-end Internet of Things (IoT) cloud solution for sensor-based endpoint devices. An RX65N-based design enables sensor data transmission over Wi-Fi or Ethernet and allows users to monitor and control smart meters as well as building and industrial automation systems using a PC dashboard.
Developers can jumpstart their designs with the RX65N Renesas Starter Kit that includes a RX65N MCU with 2MB code flash memory, an LCD display module, on-chip debugging emulator, and e2 studio integrated development environment. The kit lets designers edit and debug the sample software qualified to run Amazon FreeRTOS on the RX65N MCU. Using Amazon FreeRTOS, developers can more securely deploy an RX65N MCU-based endpoint device without having to worry about the complexity of scaling across millions of devices. Once connected to the cloud, IoT endpoint device applications can take advantage of all of the cloud’s capabilities or continue processing data locally with AWS IoT Greengrass.
For full article, please access link via : https://www.renesas.com/sg/en/products/microcontrollers-microprocessors/rx/rx600/rx65n-651.html