topics
Renesas Electronics Introduces True Bidirectional Synchronous Buck-Boost Controllers for Industrial Battery-Powered Applications
Renesas Electronics Introduces True Bidirectional Synchronous Buck-Boost Controllers for Industrial Battery-Powered Applications
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced an innovative new family of bidirectional four-switch synchronous buck-boost controllers. The ISL81601 and ISL81401 are the industry’s only true bidirectional controllers that sense peak current at both ends and provide cycle-by-cycle current limit in both directions while in buck or boost mode. The controllers generate point-of-load (POL) and voltage rail conversions with peak efficiency up to 99 percent. The ISL81601 has a wide input range of 4.5V to 60V and produces a 0.8V to 60V output to support most industrial batteries: 12V, 24V, 36V and 48V. Also available is the ISL81401, a 4.5V to 40V input and 0.8V to 40V output version, and its unidirectional counterpart, the ISL81401A. The new controllers are well suited for DC power backup and battery-powered medical, industrial and telecommunication systems.
Please visit URL for full article : https://www.renesas.com/sg/en/about/press-center/news/2018/news20181003.html