topics
Renesas Electronics Introduces Integrated Open Image Signal Processor Solution for Automotive Camera System Development with MM Solutions
Renesas Electronics Introduces Integrated Open Image Signal Processor Solution for Automotive Camera System Development with MM Solutions
Tokyo, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced an integrated open image signal processor (ISP) solution to further ease and speed the development of automotive smart camera applications based on the Renesas high-performance R-Car V3M and R-Car V3H System-on-Chips (SoCs). Integrating the ISP on the R-Car V3x SoCs and leveraging MM Solutions’ Automotive Camera Development Kit (AutoCDK), the open ISP solution on R-Car SoCs enables automotive Tier 1s to simplify the sensor calibration and tuning process for camera applications, including front camera and surround view, offering high flexibility and faster time to market in this competitive industry. Renesas will demonstrate the Open ISP Solution using the Renesas R-Car V3M, MM Solutions’ AutoCDK, and Sony’s IMX390 image sensor in booth 6 at AutoSens 2018, September 17-20, 2018, Brussels, Belgium.
For full article, please access link via : https://www.renesas.com/sg/en/about/press-center/news/2018/news20180918.html