topics
Renesas Electronics Introduces ISL91302B, ISL91301A, and ISL91301B Multiphase PMICs with Highest Efficiency and Smallest Footprint
Renesas Electronics Introduces ISL91302B, ISL91301A, and ISL91301B Multiphase PMICs with Highest Efficiency and Smallest Footprint
TOKYO, Japan, April 25, 2018 – Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced three programmable power management ICs (PMICs) that offer the highest power efficiency and smallest footprint for application processors in smartphones and tablets: the ISL91302B, ISL91301A, and ISL91301B PMICs. The PMICs also deliver power to artificial intelligence (AI) processors, FPGAs, and industrial microprocessors (MPUs), and they are ideal for powering the supply rails in solid-state drives (SSDs), optical transceivers, and a wide range of consumer, industrial and networking devices. The ISL91302B dual/single output, multiphase PMIC provides up to 20A of output current and 94 percent peak efficiency in a 70mm2 solution size that is more than 40 percent smaller than competitive PMICs (Note).
For full article, please access link via : https://www.renesas.com/en-hq/about/press-center/news/2018/news20180425.html