topics
Renesas Electronics Unveils World’s First On-Chip Flash Memory Microcontroller Featuring Advanced 28nm Embedded Flash Technology
Renesas Electronics Unveils World’s First On-Chip Flash Memory Microcontroller Featuring Advanced 28nm Embedded Flash Technology
TOKYO, Japan, March 27, 2018 ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the sample shipment of the industry’s first on-chip flash memory microcontroller (MCU) using a 28 nanometer (nm) process technology. To contribute to the realization of next-generation green cars and autonomous vehicles with higher efficiency and higher reliability, the revolutionary RH850/E2x Series MCU incorporates up to six 400 megahertz (MHz) CPU cores, which makes it the first on-chip flash memory automotive MCU to achieve the industry’s highest processing performance (Note 1) of 9600 MIPS (Note 2). The new MCU series also features a built-in flash memory of up to 16 megabytes (MB) as well as enhanced security functions and functional safety.
For further info, please access link via :https://www.renesas.com/en-hq/about/press-center/news/2018/news20180327.html