topics
Renesas Electronics Ships New RV2X6376A Series of 25 Gbps Directly Modulated Laser Diodes for 4.9G and 5G LTE Base Stations
Renesas Electronics Ships New RV2X6376A Series of 25 Gbps Directly Modulated Laser Diodes for 4.9G and 5G LTE Base Stations
TOKYO, Japan, March 13, 2018 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the RV2X6376A Series of directly modulated laser (DML) diodes. The DML diodes deliver 25 Gbps x four wavelengths as the light source in 100 Gbps optical transceivers that enable high-speed communications inside 4.9G and 5G LTE base stations, and between data center routers and servers. The RV2X6376A Series are the industry’s first DML diodes that support full 25 Gbps speed (per individual laser) and industrial temperature (-40°C to 95°C) without cooling.
For further info, please access link below:
https://www.renesas.com/en-hq/about/press-center/news/2018/news20180313.html