topics


Renesas Electronics Simplifies Integration for Industrial Ethernet with Intelligent RJ45 Module Solution

Renesas Electronics Simplifies Integration for Industrial Ethernet with Intelligent RJ45 Module Solution

üsseldorf, February 27, 2018 – Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced its latest industrial Ethernet module solution, the I-RJ45, which incorporates a single- or dual-port RJ45 connector and simplifies integration for industrial Ethernet by supporting various industrial network slave applications including sensors and transmitters, gateways, operator terminals and remote I/O. The solution comprises an intelligent RJ45 module that comes with qualified embedded software to support multiple industrial Ethernet protocol stacks. The software package and sample codes provide system manufacturers with a complete set of tools and frameworks to build their application without any additional up-front costs or complexity. This accelerates prototyping, reducing the time needed for industrial network protocol integration efforts up to three months.

Please access link below for further information:
https://www.renesas.com/en-hq/about/press-center/news/2018/news20180227c.html