topics
Renesas Electronics Delivers R9J02G012 Controller That Enables Device-to-Device Authentication in Support of Safer USB Power Delivery Ecosystem
Renesas Electronics Delivers R9J02G012 Controller That Enables Device-to-Device Authentication in Support of Safer USB Power Delivery Ecosystem
Industry’s First USB Power Delivery Controller Supporting Both USB PD Rev. 3.0 and USB Type-C™ Authentication Rev 1.0 in a Single Package
Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced its new R9J02G012 USB Power Delivery (USB PD) controller intended for use in a wide range of USB PD products employing direct current (DC) power including AC adapters, PCs, smartphones, other consumer and office equipment, and toys. The R9J02G012 is the industry’s first single package solution (Note 1) that supports both USB Power Delivery Rev. 3.0 (USB PD 3.0) and USB Type-C™ Authentication Rev 1.0, which enables device-to-device authentication.
Detail available at https://www.renesas.com/en-hq/about/press-center/news/2017/news20170530.html