topics
Renesas R-Car Starter Kit Adopted as a Standard Reference Platform for Automotive Grade Linux to Accelerate IVI Development for Next-Generation Connected Cars
Renesas R-Car Starter Kit Adopted as a Standard Reference Platform for Automotive Grade Linux to Accelerate IVI Development for Next-Generation Connected Cars
R-Car Starter Kit Supports the Latest Unified Code Base 3.0 64-Bit Software Environment
Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced that Automotive Grade Linux (AGL) has adopted the Renesas R-Car Starter Kit as one of its standard reference platforms for software development. AGL is a collaborative open source project that is bringing together automakers, suppliers and technology companies to build a Linux-based, open software platform for automotive applications that can serve as the de facto industry standard. Its adoption of the Renesas R-Car Starter Kit makes it easy for software developers to acquire the hardware environment that runs software developed by this project and allows them to quickly and easily develop in-vehicle infotainment (IVI) application software for next-generation connected cars.
Detail available at https://www.renesas.com/en-hq/about/press-center/news/2017/news20170524.html