topics


Renesas Electronics Introduces 32-Bit Automotive Microcontrollers Specialized for Instrument Clusters in Entry Level to Mid-Range Cars

Renesas Electronics Introduces 32-Bit Automotive Microcontrollers Specialized for Instrument Clusters in Entry Level to Mid-Range Cars

Renesas Electronics Corporation, a premier supplier of advanced semiconductor solutions, today announced the RH850/D1x Series of 32-bit automotive microcontrollers (MCUs) specialized for instrument clusters that deliver easy-to-access information to support a safer and rich driving experience.
The connected car is generating amount of information from the automotive networks, cameras and multimedia systems. This trend drives a strong needs to transmit these large amounts of information to the driver in an easy-to-understand and easy-to-read manner, with a graphical expression. As graphics become widely used in instrument clusters, color LCDs are going to be widely adopted to increase both the expressive power and legibility, improving the communications with driver to provide appropriate information at the appropriate time with appropriate displays through a combination of gauges, graphics, and head-up display.
For more detail, please visit the following url.
http://www.renesas.com/press/news/2015/news20150220.jsp