topics
Renesas Electronics Expands True Low Power™ RX111 Group Microcontroller Lineup within the 32-Bit RX Family with Larger Memory Capacities up to 512 KB
Renesas Electronics Expands True Low Power™ RX111 Group Microcontroller Lineup within the 32-Bit RX Family with Larger Memory Capacities up to 512 KB
Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the addition of new product versions with larger memory capacity to the RX111 Group of 32-bit microcontrollers (MCUs) ideal for applications such as healthcare devices, industrial equipment, and building automation systems.
Renesas’ existing RX111 Group product lineup offer package pin counts of 36 to 64 pins, flash memory capacity of 16 KB to 128 KB, and RAM capacity of 8 KB to 16 KB. The new product versions extend the flash memory capacity range to 512 KB and the RAM capacity range to 64 KB. The total number of product versions will grow from 31 to 46, strengthening the RX111 Group product lineup overall.
For more detail, please visit following URL.
http://www.renesas.com/press/news/2014/news20140929.jsp