topics
Renesas Electronics RX72M Solution Supports the Major Protocols and Significantly Reduces Development Time for Slave Equipment in Industrial Network
Renesas Electronics RX72M Solution Supports the Major Protocols and Significantly Reduces Development Time for Slave Equipment in Industrial Network
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the development of the RX72M Industrial Network Solution to accelerate the development of industrial slave equipment using the RX72M Group of 32-bit industrial Ethernet microcontrollers (MCUs).
The new RX72M solution includes an evaluation board, an operating system, middleware, and a sample software that supports approximately 70 percent of the communications protocols used in industrial network applications. This enables users to immediately launch slave equipment development, such as motor control blocks for compact industrial robots, PLC (programmable logic controller) devices, and remote I/O systems. The sample software includes: EtherCAT, PROFINET RT, Ethernet/IP, Modbus TCP, and OPC UA, as industrial Ethernet software, and PROFIBUS DP, Modbus, RTU/ASCII, CAN open, and DeviceNet, as Field Bus communication software.
Renesas has confirmed conformance testing for the three major protocols – EtherCAT, PROFINET RT, and Ethernet/IP – which represents the global industrial Ethernet market. This allows developers to reduce the overall development time – including development, evaluation, and verification steps – by as much as six months, accelerating their time to market.
For full article, please access the link : https://www.renesas.com/sg/en/about/press-center/news/2019/news20190911.html