2014
Topics 2014
2014.12.1 Renesas Electronics Introduces the RX113 Group of 32-Bit Microcontrollers for Healthcare Equipment, Home Appliances and Industrial Equipment
TOKYO, Japan, December 1, 2014 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, is expanding the use of touch key in healthcare, building automation and home appliance applications with the new RX113 Group of microcontrollers (MCUs). Part of the RX100 Series, the new MCUs offer a single-chip solution with unique touch sensor IP and leading-edge low-power technologies. This enables significantly reduced power, size, and development costs for entry-level devices in these markets, as well as for other cost-sensitive, capacitive touch-based applications for the growing Internet of Things (IoT) market. Renesas’ innovative touch sensor intellectual property (IP) core achieves both high noise immunity and high sensitivity, offering touch key operation on wet and curved touch panels.
For more detail, please visit the following URL.
http://www.renesas.com/press/news/2014/news20141201.jsp
2014.11.9 Renesas Electronics Eases Safety, Security, and Connectivity for the Car of the Future
All-in-One Solution Delivers Functional Safety, Encryption, Performance and Communications for Driver Assistance Systems That Enable Self-Driving Cars
Renesas Electronics Corporation, a premier supplier of advanced semiconductor solutions, is easing the design complexities involved in developing self-driving car and other driver assistance systems that can offer users with a safe, secure, and convenient driving experience. The new RH850/P1x-C Series, a high-end version of the RH850/P1x Series of 32-bit automotive microcontrollers (MCUs), is designed for sensor fusion, gateway, and advanced chassis system applications that will enable the types of advanced systems envisioned in the car of the future.
For more detail, please visit the following URL.
http://www.renesas.com/press/news/2014/news20141106.jsp
2014.11.9 Renesas Electronics Delivers Enhanced User Experience with Integrated Automotive Cockpit Solution
TOKYO, Japan, October 22, 2014 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, is enhancing the driving experience with robust new solutions for the integrated car cockpit. As the newest member of Renesas’ state-of-the-art R-Car Series for automotive, the R-Car E2 automotive systems-on-chip (SoCs) and the new R-Car E2 software development board deliver optimized infotainment and display audio for entry-level integrated cockpit systems that support smartphone interoperability and, in combination with other Renesas R-Car Series devices, help achieve the scalability required to bridge the full range of integrated cockpit systems from entry-level to high-end models.
In an integrated cockpit, the converged system integrates and analyzes multiple streams of information and reports the results to the driver in an optimized format, which is increasingly delivered through interoperation with smartphones. This convergence is driving demand for higher level functionality and greater added value for entry-level applications.
For more detail, please visit following URL.
http://www.renesas.com/press/news/2014/news20141022.jsp
2014.10.12 Renesas Electronics Expands True Low Power™ RX111 Group Microcontroller Lineup within the 32-Bit RX Family with Larger Memory Capacities up to 512 KB
Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the addition of new product versions with larger memory capacity to the RX111 Group of 32-bit microcontrollers (MCUs) ideal for applications such as healthcare devices, industrial equipment, and building automation systems.
Renesas’ existing RX111 Group product lineup offer package pin counts of 36 to 64 pins, flash memory capacity of 16 KB to 128 KB, and RAM capacity of 8 KB to 16 KB. The new product versions extend the flash memory capacity range to 512 KB and the RAM capacity range to 64 KB. The total number of product versions will grow from 31 to 46, strengthening the RX111 Group product lineup overall.
For more detail, please visit following URL.
http://www.renesas.com/press/news/2014/news20140929.jsp
2014.9.13 Renesas Electronics New R-Car V2H Device Offers High-Resolution Image Recognition for Safer Driver Assistance Systems in Conventional and Emerging Self-Driving Vehicles
Renesas Electronics Corporation (TSE: 6723), today announced the availability of its R-Car V2H, the company’s newest system-on-a-chip (SoC) implementing state-of-the-art image recognition technology to support high-resolution surround viewing in advanced driver assistance systems (ADAS). This is the first R-Car ADAS device from Renesas and includes additional functionality for higher performance, lower power, and improved safety in traditional and emerging self-driving vehicles.
For more detail, please visit following url;
http://www.renesas.com/press/news/2014/news20140828.jsp
2014.9.13 Renesas Electronics Announces New 40 nm RH850/C1x Series of Microcontrollers for HEV/EV Motor Control Applications
Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the new RH850/C1x Series of 32-bit microcontrollers (MCUs), designed for motor control in hybrid electric vehicles (HEVs) and electric vehicles (EVs). Based on Renesas Electronics’ 40-nanometer (nm) process, the RH850/C1x Series features the RH850/C1H and RH850/C1M MCUs, which enable embedded designers to enhance efficiency, reduce system costs, and achieve higher safety levels for HEV/EV motor control systems.
For more detail, please visit following site:
http://www.renesas.com/press/news/2014/news20140827.jsp
2014.9.13 Renesas Electronics Introduces RX631, RX63N Safety Package Solution that Accelerates Implementation of Functional Safety Systems for Industrial Equipment
Renesas Electronics Corporation, a premier supplier of advanced semiconductor solutions, today announced that it has obtained IEC61508 (Functional Safety) certification for the RX631, RX63N Safety Package, featuring a robust self-diagnostic software and a safety manual for microcontrollers (MCUs) necessary to implement functional safety in industrial equipment. An RX631, RX63N Safety Solution Evaluation Kit will be available in November 2014, providing a hardware evaluation board with the RX63N MCU, the evaluation version of the self-diagnostic software library, and a Users Guide.
For more detail, please visit our web site below;
http://www.renesas.com/press/news/2014/news20140826.jsp
2014.8.20 Renesas Electronics Expands Portfolio of Simple Power Supply ICs with Innovative Wide Input DC/DC Regulators Targeting Smart Grid and Industrial Applications
TOKYO, Japan, August 19, 2014 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today expands its portfolio of Simple Power Supply ICs, with innovative 16V input capable synchronous buck regulators that deliver up to 3A continuous current to loads at voltages as low as 0.8V. The new power supply ICs are ideal for systems requiring even lower power consumption in standby mode, and systems requiring backup power in case of power outage. The devices target applications in the industrial, office equipment, consumer, networking, smart grid, and other fields.
By reducing the power supply design workload, the new devices lower power consumption and improve the compactness of the overall system for improved power efficiency and lower BOM cost. The new Simple Power Supply ICs are available in four series with different DC/DC converter output counts and output voltages. Battery backup functionality is availability in the: RAA23012X series, RAA23013X series, RAA23022X series, and the RAA23023X series. Each series comprises three product versions, for a total of 12 new devices.
As systems become more power efficient and compact in recent years, demand has grown for power supply blocks with improved power efficiency delivered in a compact form factor. One commonly used method of reducing power consumption is to incorporate a low-power mode in which only the functions needed in the microcontroller’s (MCU) standby state continues to operate. Unlike MCUs, however, such measures are rarely implemented within the power supply block itself. The common method of using a pair of diodes to implement a battery backup circuit for devices such as SRAM and MCUs, which require power even when the system is powered down, makes it difficult to maintain a compact system. What is more, in systems that require two or more voltages, the usual method is to employ multiple single-output power supply ICs or electronic components, which also presents a barrier to compactness.
For more detail, please visit following URL.
http://www.renesas.com/press/news/2014/news20140819.jsp
2014.8.18 Renesas Electronics Issues New Business Direction Presentation “Renesas Efforts towards Further Growth in Profits”
TOKYO, Japan, August 6, 2014 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced its new business direction and issued its corporate presentation titled “Renesas Efforts towards Further Growth in Profits.”
Refer to the “Renesas Efforts towards Further Growth in Profits” presentation document for full information about Renesas’ new business direction at following URL.
http://www.renesas.com/press/news/2014/news20140806d.jsp
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.
pagetop2014.7.21 Renesas Electronics Intellectual Property for Capacitive Touch Sensing Delivers Industry-Leading Performance for Human Machine Interface Applications
Renesas Electronics Corporation, July 15th announced development of innovative new intellectual property (IP) that implements industry-leading capacitive touch sensing technology suitable for home appliances, and healthcare equipment, such as blood pressure and blood glucose meters. The IP achieves high-touch sensitivity five times superior compared to that of Renesas’ R8C/3xT microcontrollers (MCUs), as well as high-noise immunity allowing the technology to pass strict noise tests. Furthermore, for the first time, Renesas IP supports the mutual capacitance method which is more reliable and versatile than the common self-capacitance method. Renesas will also provide development tools to make application development easier.
For more detail, please visit following URL.
http://www.renesas.com/press/news/2014/news20140715.jsp